Technical FAQs

Ask a Question

How do you enable upload / download a SoMachine appplication with a M258 Controller?

Procedure to download Source Project:
1) Connect to the controller
2) Download the latest version of the application to the project
3) Stop the Controller
4) While Login and the controller stop, download the source project
5) Start the Controller

Procedure to upload the Source Project:
1) Create a new test project with the same M238/M258 model
2) Connect to the controller with downloading any changes
3) Stop the controller
4) While Login and the controller stop, upload the source project

Was this helpful?
What can we do to improve the information ?