Technical FAQs

Ask a Question

What should I do to clear the Deviation fault 1 and / or 2 on CAY modules?

To clear these faults go to adjust screen set the parameters for error 1 and 2 to zero. When you have optimized your system you may enter a valid value related to your application.
During the commissioning phase if the servo system is not optimized it is normal for this error to occur.


Legacy KB System (APS) Data: RESL2079 V2.0, Originally authored by RiTa on 03/17/2012, Last Edited by MiOB on 03/17/2012
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?