Technical FAQs

Ask a Question

Can I use a BMXNOM0200 module in a M340 BMXPRA0100 rack?

Yes, you can have a maximum of 4 configured serial link ports using 2 to 4 modules. Please refer to the BMXPRA0100 User Guide, in the section on Restricted Capabilities of a Remote I/O Station BMXPRA0100, under Communication Capabilities.


Legacy KB System (APS) Data: RESL207663 V1.0, Originally authored by DaSo on 04/20/2012, Last Edited by DaSo on 04/20/2012
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?