Technical FAQs

Ask a Question

Correction to Published Specifications on the 499NES25100 Switch

Goals and Symptoms

Current catalogs and manuals incorrectly state the temperature range of the 499NES25100 unmanaged switch as being -40C to 70C. The purpose of this Resolution is to notify users of this product of the correct range.

Causes and Fixes

The correct temperature range is
Operating Range 0C-60C
Storage Temperature -20C to 85C

Attachments

(Removed File URL: 207593_22A6/data_sheet_-_499n_unmanaged_switch.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/d3437be6a930e095c12579ba0016108f/fl_block_5/0.114?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL207593 V1.0, Originally authored by PeZa on 03/07/2012, Last Edited by PeZa on 03/07/2012
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?