Technical FAQs

Ask a Question

Does Schneider Electric offer the CANbus fieldbus cables used to connect to the Berger Lahr D065 and N065 motors?

Fieldbus cables and connectors used for the (Berger Lahr ) D065 and N065 motors are PRODUCTS made by third party vendors and are not offered by Schneider Electric.
Connectors and cables for these motors can be purchased from Turck USA.
A couple examples of these items from Turck USA can be seen at the web addresses shown below.


http://www.turck-usa.com/illustrations/B2007_D89.pdf - This is an example of the CANbus connector that will interface with D065 or N065 motors. See item CMB 8251-0

http://www.turck-usa.com/illustrations/B2007_D11.pdf - This is an example of a CANbus cable that will interface with D065 and N065 motors. See item WK 4.5T-*/S90

Was this helpful?
What can we do to improve the information ?