Technical FAQs

Ask a Question

With Lexium 32 M, can the speed of a point to point position move be controlled via the optional Analog input?

No, it is not possible to control the speed of a movement via the optional analog input in Point to Point operating modes such as "MoveAbsolute or MoveRelative.
This is true for all operating modes which make point to point movement which includes Motion Sequence mode.


Legacy KB System (APS) Data: RESL207417 V1.0, Originally authored by TVe on 02/16/2012, Last Edited by TVe on 02/16/2012
Related ranges: Lexium 32
Was this helpful?
What can we do to improve the information ?