Technical FAQs

Ask a Question

Is the 'A' or 'B' PLC designation selectable in a Unity 140CPU67160 Hot Standby system?

Yes. As of firmware version 3.00-00-42 the 'A' or 'B' designation can be selected by using the LCD panel. The setting can be found by navigating to the PLC Operations - Hot Standby area.
***Using firmware versions previous to this the 'A' and 'B' designation was determined by the MAC address found on the lower front of the PLC. With both PLCs on-line, the lowest MAC address was 'A'.


Legacy KB System (APS) Data: RESL207391 V1.0, Originally authored by DaSo on 02/14/2012, Last Edited by DaSo on 02/14/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?