Technical FAQs

Ask a Question

Is it possible to simulate a discrete input (%I) in Unity?

Yes. Use the WRITE_INPUT_EBOOL block.


Legacy KB System (APS) Data: RESL207273 V1.0, Originally authored by DaSo on 02/01/2012, Last Edited by DaSo on 02/01/2012
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?