Technical FAQs

Ask a Question

Is there a Quantum hardware solution for AS- i V2.x PRODUCTS?

Yes. There is an Ethernet / AS-I Gateway offered by Schneider which will allow you to interface AS-i V2.x product. The part number for the gateway is TCSACEA1SF13F. The user manual is attached here. tcsagea1sf13f_manual.zip


Legacy KB System (APS) Data: RESL207231 V1.0, Originally authored by DaSo on 01/26/2012, Last Edited by DaSo on 01/26/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?