Technical FAQs

Ask a Question

How can I copy multiple Genie, Supergenie, Symbol and template library files between Vijeo Citect V7.2 applications.

There are following library files residing inside project folder and they can be just copied/pasted across different projects.

.CTM file  - Genie or Supergenie library
.CTL file - Symbol library
.CTT file - template library

You can copy these files from one project and can paste into another project folder where you want to use them. Make sure to then pack the project -> Pack libraries -> Update pages -> Compile project (by turning off Increment compile) to restore those files into new project.

Was this helpful?
What can we do to improve the information ?