Technical FAQs

Ask a Question

TSXWMY modules takes 2 minutes to start.

Goals and Symptoms

TSXWMY100 modules takes 2 minutes to start

Facts and Changes

TSXWMY100

Causes and Fixes

The TSXWMY100 takes up to 2 minutes to completely start.
Due to the amount of services and the application size configured on the module, it can take awhile
for the 'TSXWMY100 to completely start up. The reason is because each service must perform checks
to ensure that the external referenced databases exist

This works as designed.


Legacy KB System (APS) Data: RESL206623 V1.0, Originally authored by AlCh on 11/10/2011, Last Edited by AlCh on 11/10/2011
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?