Technical FAQs

Ask a Question

What is the maximum number of serial communications modules, BMXNOM0200, that may be configured in an M340 system?

A M340 BMXP3420xx version 2.x processor can support a maximum of 36 Application Specific Channels.
Each BMXNOM0200 module is counted as 2 Application Specific Channels. This gives a maximum potential of 18 BMXNOM0200 modules.


Legacy KB System (APS) Data: RESL206248 V1.0, Originally authored by MiMe on 09/27/2011, Last Edited by MiMe on 09/27/2011
Related ranges: Modbus
Was this helpful?
What can we do to improve the information ?