Technical FAQs

Ask a Question

How to connect the XBT H/P/E/F to the PLC Siemens S7-300?

Goals and Symptoms

How to connect the XBTF to the PLC Siemens S7-300?

Facts and Changes

The cable XBTZ979 is no longer available on the Schneider Catalogue

Causes and Fixes

The R&D has validated the following adaptor:

<< (HELMHOLZ 700-751-1VK21 SSW7, Converter for MPI-Bus (PC-Converter) >>, in order to replace the cable XBTZ979.

Attached, please find the procedure on how to use the adaptor so as to connect a XBT to the PLC Siemens S7-300.

This fix concerns the following terminals:

XBT-H
XBT-P
XBT-E
XBT-HM
XBT-PM
XBT-F
XBT-FC

XBTF_To_SiemensS7_PLC_MPI_Connection.zip


Legacy KB System (APS) Data: RESL206039 V1.0, Originally authored by MaLy on 08/23/2011, Last Edited by MaLy on 08/23/2011
Related ranges: Magelis XBT H, XBT P, XBT E, Magelis XBT F, TXBT F
Was this helpful?
What can we do to improve the information ?