Technical FAQs

Ask a Question

Unity Pro v6.0 LL984 Editor. Installed LL984 editor but it is not available in the library.

The Custom Library folder in the <Tools><Options><Paths> should be point to:
C:\Documents and Settings\All Users\Schneider Electric\ApplicationData\UnityPro\CustomLibset\v6.0


Legacy KB System (APS) Data: RESL206034 V1.0, Originally authored by DaSo on 01/03/2012, Last Edited by DaSo on 01/03/2012
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?