Technical FAQs

Ask a Question

What does halt code 8A57 mean in the M340's system word %SW125?

The meaning of the HALT code 8A57 is: E_ERR_NULL_INPUT_SCALE.
It is an application issue. The EF (elementary function) may have invalid data. The error is detected when the
online modification validation is performed. Perform an Analyze project to find the cause of the error.


Legacy KB System (APS) Data: RESL205470 V1.0, Originally authored by DaSo on 06/08/2011, Last Edited by DaSo on 06/08/2011
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?