Technical FAQs

Ask a Question

Do the I/O screw terminals connectors come with the Modicon M340 I/O modules or do they have to be ordered separately?

Yes, the I/O screw terminal connectors have to be ordered separately for the Modicon M340 I/O modules. Is some cases, you may only have the option to order a cable with a connector on one end and a pigtail of wires on the other end or a cable with connectors on both ends end to connect to a compatible Telefast block.


Legacy KB System (APS) Data: RESL205260 V1.0, Originally authored by DaSo on 05/19/2011, Last Edited by DaSo on 05/19/2011
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?