Technical FAQs

Ask a Question

Can you configure a new Modicon M340 over Modbus with Unity Pro? If so, what are the default communication parameters for the Modbus port?

Yes, you can connect to a new Modicon M340 CPU via Modbus. The Modbus port parameters are RS485, 19200 baud, 8 data bits, even parity, 1 stop bit. So you need a RS485 Modbus network (at 19200 baud) to connect to an M340 CPU with defaut parameters on Modbus port. Otherwise, you have to choose a different communication method (USB or Ethernet, for example) and configure the Modbus port parameters in the application.


Legacy KB System (APS) Data: RESL205259 V1.0, Originally authored by DaSo on 05/24/2011, Last Edited by DaSo on 05/24/2011
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?