Technical FAQs

Ask a Question

When should I consider increasing the amount of SRAM in my Unity Quantum application?

Once your application has consumed 90% of free memory it is recommended that you increase the amount of available SRAM.


Legacy KB System (APS) Data: RESL205114 V1.0, Originally authored by TVe on 04/16/2011, Last Edited by TVe on 04/16/2011
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?