Technical FAQs

Ask a Question

Is there a specific percentage of memory fragmentation that would require running the PACK command?

We recommend running the PACK command when fragmentation exceeds 5%.


Legacy KB System (APS) Data: RESL205106 V1.0, Originally authored by TVe on 04/16/2011, Last Edited by TVe on 04/16/2011
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?