Technical FAQs

Ask a Question

At what point during the PLC scan are the values in an Animation Table or animated logic section updated?

The values are updated at end of scan.


Legacy KB System (APS) Data: RESL204799 V1.0, Originally authored by DaSo on 03/11/2011, Last Edited by DaSo on 03/11/2011
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?