Technical FAQs

Ask a Question

Do I have to power cycle the PLC in order to recognize a switch change from RTU to MEM on the 140NOM21200?

If your using a Unity Quantum PLC you will have to cycle power. If your using a Non Unity Quantum PLC you will not have to perform a power cycle.


Legacy KB System (APS) Data: RESL204695 V1.0, Originally authored by DaSo on 03/03/2011, Last Edited by DaSo on 03/03/2011
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?