Technical FAQs

Ask a Question

How can I see the entire program of a Model 50 and 30 CPU with SFW 50 and SFW 30 software when many of the rungs are unable to be displayed?

Even if the rungs can not be displayed with the SFW 50 or SFW 30 software, you can print the rung logic in Boolean format. By printing the program in Boolean you can now view the rungs that were not displayed in the software.


Legacy KB System (APS) Data: RESL2045 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?