Technical FAQs

Ask a Question

How to transfer a Factorycast configuration to a Web Designer application

Goals and Symptoms

How to convert a Factorycast configuration to a Web Designer application.

Facts and Changes

Web Designer

Causes and Fixes

There is no direct method available for converting a Factorycast application to a Web Designer
application. (i.e., TestProject.cfg, etc.). In order to convert the Factorycast application to a Web Designer
application, the Factorycast configuration file and web pages must be separately imported.



The following steps can be used to convert a Factorycast configuration to a Web Designer
application.

  • Start Web Designer.
  • Click on 'Project\Inport'.

  • Click on the selection named 'Factorycast project.

  • Click on the selection for the applicable NOE version (i.e.,NOE771 11 v4.5)
  • Click on the 'Browse' button.

  • Browse for the Factorycast configuration
  • Click on the configuration name.
  • Click on 'Open'


  • Click on the 'Finish' button to start the import.


To view the symbols after the import finishes,
  • Click on 'Devices'
  • Click on the Device name.
  • Click on 'the Variables' tab.


To import the web pages,
  • Right click on the location where the web pages are to be imported to.
  • Click on 'Import File'.


  • Browse for the custom web page file
  • Click on the 'Open' button.
  • Repeat the last four steps for the other custom web pages.
Was this helpful?
What can we do to improve the information ?