Technical FAQs

Ask a Question

What happens to a Concept Compact project when it is imported into Unity V5.1 S which only supports the M340 PLC line?

When Unity imports a Concept Compact PLC project into Unity, it will try to convert the project to a Quantum PLC.
Since Unity Pro S only suppports the M340 PLC line, the import returns an error:

" The configuration catalog is not compatible with the current application:
Some Objects are missing or the version is incompatible.: The Required CPU reference: <140CPU53414A/U 01.00 > is MISSING.
Import failed [ 1 error[s], 0 warning[s]]"


Legacy KB System (APS) Data: RESL204332 V1.0, Originally authored by DaSo on 02/02/2011, Last Edited by DaSo on 02/02/2011
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?