Technical FAQs

Ask a Question

What is the SCCR (Short Circuit Current Rating) for the Lexium 15 drives?

The SCCR (Short Circuit Current Rating) for the Lexium 15 drives is 42kA.


Legacy KB System (APS) Data: RESL204209 V1.0, Originally authored by TVe on 12/23/2010, Last Edited by TVe on 12/23/2010
Related ranges: Lexium 15
Was this helpful?
What can we do to improve the information ?