Technical FAQs

Ask a Question

Can the Advantys OTB Communicate with the TSXETY110 module.

Goals and Symptoms


Can the Advantys OTB be used to communicate with the TSXETY110 module.

Causes and Fixes


Can the Advantys OTB be used to communicate with the TSXETY110 module?

The answer is no, the Advantys OTB cannot be used to communicate with the TSXETY110 module

The Advantys OTB uses 'Modbus TCP/IP' for the communications protocol.
The Premium ETY110 module uses 'XWAY' Ethernet for the communications protocol.


Legacy KB System (APS) Data: RESL204180 V1.0, Originally authored by AlCh on 12/16/2010, Last Edited by AlCh on 12/16/2010
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?