Technical FAQs

Ask a Question

Unity returns 'DTM device not found' error.

Goals and Symptoms

'Unity' returns a 'DTM device not found' error when you try to add an 'Ethernet IP' NOE or ETY to the rack.

Facts and Changes

Unity 5.0

Causes and Fixes


'Unity' returns a 'DTM device not found' error when you try to add an 'Ethernet IP' NOE or ETY to the rack.

The problem is happening because the 'DTM' software has not been installed and properly setup.

The following steps can be used to resolve the issue:

  • Shutdown Unity.
  • Install the latest hot fixes for Untiy 5.0.

Hot fix 'unitypro_v50_hf20047096' can be downloaded from:
http://www.global-download.schneider-electric.com/8525773E00058BDC/all/EDCD223194AC6
B6B85257799006B8B43/$File/unitypro_v50_hf20047096.zip


Hot fix ' unitypro_v50_hf1' can be downloaded from:
http://www.global-download.schneider-electric.com/8525773E00058BDC/all/95E16F40DFB8521
A85257789005A3275/$File/unitypro_v50_hf1.zip
  • Install the 'Unity Pro Ethernet Configuration Tool' (This is on a CD that is shipped witht he module.)
  • Install the 'Unity Pro Generic Modbus TCP DTM' (This is on the same CD in a seperate folder.).
  • Install the Unity Pro Generic EtherNet IP DTM' (This is on the same CD in a seperate folder).
  • Start 'Unity'.
  • Open the 'Unity' application.
  • Click on 'Tool\Hardware Catalog'
  • Click on 'DTM Catalog'
  • Click on 'External Update Tool'.
  • Click on the 'Update' button in the 'FDT/DTM Catalog' window.
  • Click on the 'OK' button in the message window that appears after the update finishes.


Click on the 'Close' button to close the 'FDT/DTM Catalog' window.
  • Click on the 'Reload catalog' button.
  • Add the Ethernet IP module to the rack.

Legacy KB System (APS) Data: RESL203481 V1.0, Originally authored by AlCh on 09/21/2010, Last Edited by AlCh on 09/21/2010
Related ranges: Modicon Premium, Modicon Quantum
Was this helpful?
What can we do to improve the information ?