Technical FAQs

Ask a Question

Is there an easy way to load all the libraries required for the CANopen Motion Bus in MotionPro?

Yes, there is. In the MotionPro software, go to Window \ Library Manage. Right-click in the Library Manager window and select "Additional Library...". Select LMC_NewSoftmotionProject.lib library from the following folder C:\Program Files\Schneider Electric\Motion Control\CoDeSys V2.3\Targets\Schneider Electric\Lexium Controller V0106\Library. This will load all the required libraries for the CANopen Motion Bus


Legacy KB System (APS) Data: RESL203046 V1.0, Originally authored by TVe on 08/04/2010, Last Edited by TVe on 08/04/2010
Related ranges: Lexium Controller LMC10 - LMC20
Was this helpful?
What can we do to improve the information ?