Technical FAQs

Ask a Question

Why don't I see the memory words used in the ProWORX 32 logic editor window?

This first screen shot shows where the "memory words used" information is missing.....

This is because the Network Navigator window is closed. Once you open the Network Navigator window, the "memory words used" information will appear. The PLC memory usage can be found in the Logic Editor window. At the bottom of the screen there's a gray bar that lists the memory words used along with capacity. The first number is the memory words used and the number after the "/" indicates the total memory words available for the PLC.


Legacy KB System (APS) Data: RESL203019 V1.0, Originally authored by RoAl on 07/29/2010, Last Edited by RoAl on 07/29/2010
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?