Technical FAQs

Ask a Question

How to setup RSTP on an Advantys STBNIP2311.

Release Notice
Make sure the Advantys STB NIP 2311 is updated to the minimum firmware version 3.0
Goals and Symptoms
To enable RSTP on an Advantys STB NIP 2311.
Facts and Changes
Log on to the web pages for a STBNIP2311 and Select SETUP .
Then in the left-hand menu tree select RSTP. (See graphics below)

In the Parameter window change the STATUS to Enabled.
Note:Advanced users can modify the Bridge Priority value to fine-tune the operation of the RSTP protocol.

Causes and Fixes

Legacy KB System (APS) Data: RESL203000 V2.0, Originally authored by MiMe on 07/28/2010, Last Edited by BrWa on 11/15/2012
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?