Technical FAQs

Ask a Question

Can I assign a variable to a bit within a word in Concept?

No, bit descriptors are not supported in Concept. An alternative approach would be to use a Word_To_Bit block and assign a variable names to the resulting bits of the conversion.


Legacy KB System (APS) Data: RESL202948 V1.0, Originally authored by DaSo on 07/26/2010, Last Edited by DaSo on 07/26/2010
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?