Technical FAQs

Ask a Question

What does Modsoft error "cannot open file project.MAP" mean?

This usually occurs when trying to download a project to the PLC. It is corrected by verifing that the 'read only' attribute is not
set on the project.MAP file.

Write protection on project files causes problems in downloading if the protection includes.MAP or.CUT files.
Modsoft must write to these files to process the download.
During the control logic conversion process the file 'project.MAP' is created and the ladder logic file with checksum information
is created with an .IMG extension.


Legacy KB System (APS) Data: RESL202783 V1.0, Originally authored by DaSo on 07/06/2010, Last Edited by DaSo on 07/06/2010
Related ranges: Modsoft
Was this helpful?
What can we do to improve the information ?