Technical FAQs

Ask a Question

What type of addressing are supported by simple CSV file in the Link Variable option of Vijeo Designer?

It only support 984LL addressing when linking to a simple CSV file in Vijeo Designer .


Legacy KB System (APS) Data: RESL202735 V1.0, Originally authored by GeMc on 06/25/2010, Last Edited by GeMc on 06/25/2010
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?