Technical FAQs

Ask a Question

TSXPCU1030 cable and Windows VISTA, Windows 7 compliance.


The TSXPCU1030 cable is not compliant with Windows VISTA and Windows 7.

This cable has been replaced by the TSXPCX1031 which is compliant with Windows VISTA and Windows 7.


Legacy KB System (APS) Data: RESL202374 V1.0, Originally authored by LaBa on 05/27/2010, Last Edited by LaBa on 05/27/2010
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?