Technical FAQs

Ask a Question

What is the maximum configuration for the Modular Twido Controllers?

Goals and Symptoms
To better explain the maximum configuration of the Modular Twido Controllers with I/O modules.
Causes and Fixes
The Maximum I/O configuration is between 4 and 7 I/O modules depending on the Controller model. What has to be taken into consideration when adding modules is the density of the modules, you can not exceed any of the maximum I/O points allowed. See below for the maximum counts:


NOTE: The Twido line was obsoleted 12/31/2016 and was replaced by the M221 product line, The m221 can have up to 14 modules on thelocal bus. 

Legacy KB System (APS) Data: RESL202164 V2.0, Originally authored by DiSa on 05/04/2010, Last Edited by BrWa on 12/28/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?