Technical FAQs

Ask a Question

What causes 'PrwxLoadLib Runtime error 17' when loading a loadable .DAT file using Proworx 32?

The path to the project or loadable file should not be more than 3 levels deep when using Proworx 32.


Legacy KB System (APS) Data: RESL201758 V1.0, Originally authored by DaSo on 04/19/2010, Last Edited by DaSo on 04/19/2010
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?