Technical FAQs

Ask a Question

Does a Modicon M340 CPU have to go in the slot next to the Power Supply or can it be moved to another slot?

The M340 CPU has to be in slot 0, next to power supply.


Legacy KB System (APS) Data: RESL201702 V1.0, Originally authored by DaSo on 03/25/2010, Last Edited by DaSo on 03/25/2010
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?