Technical FAQs

Ask a Question

How can I correct the "(character pos.;) E1170 data type ANY_BIT expected" error in Unity Pro when creating a variable?

Go to <Tools><Project Setttings><Variables>. Verify that the "Allow INT/DINT in place of ANY_BIT" box is checked.


Legacy KB System (APS) Data: RESL201473 V1.0, Originally authored by DaSo on 03/02/2010, Last Edited by DaSo on 03/02/2010
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?