Technical FAQs

Ask a Question

Can the serial number on an M340 SD memory card be changed?

No, the serial number of the SD card is burned into a component of the card by the manufacturer.


Legacy KB System (APS) Data: RESL201433 V1.0, Originally authored by DaSo on 02/24/2010, Last Edited by DaSo on 02/24/2010
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?