Technical FAQs

Ask a Question

Saving an IP address to a 170ENT11002’s flash ram memory with the Bootp lite tool.

Goals and Symptoms

Saving an IP address to a 170ENT11002s flash ram memory with the Bootp lite tool.

Causes and Fixes


This is a two step procedure in order to save the IP address:
First step erases the previous IP address in flash ram memory.
Second step saves the new IP address in flash ram memory.

Steps to be taken before running this procedure:
Turn off the PCs firewall and any anti virus software. ( This will allow port 502 communication)
Disable any wireless network connection.
Connect directly to the 170ENT11002 module with a crossover cable from your PC.


.


Was this helpful?
What can we do to improve the information ?