Technical FAQs

Ask a Question

Why can't I authorize TwidoSuite once the 30 day trial period has expired?

This problem can happen when the systems TEMP directory has the hidden file attributes.
In this case, you can try the following process :
Enter in DOS prompt the command "attrib %TEMP%" to check if the hidden attribute (H) is set. You can remove it with command "attrib %TEMP% -H".
You should then be able to register TwidoSuite.

Legacy KB System (APS) Data: RESL201356 V3.0, Originally authored by DiSa on 02/12/2010, Last Edited by BrWa on 01/02/2013
Related ranges: TwidoSuite
Was this helpful?
What can we do to improve the information ?