Technical FAQs

Ask a Question

Are the Modbus Port parameters configurable on the Advantys OTB (OTB1S0DM9LP) using the Advantys configuration software v4.5 ?

Only the Modbus address and baud rate are configurable via rotary switches on the unit. The remaining Modbus communication parameters are fixed at RTU, 8 data bits, Even parity, and 1 stop bit.


Legacy KB System (APS) Data: RESL201153 V1.0, Originally authored by DaSo on 01/28/2010, Last Edited by DaSo on 01/28/2010
Related ranges: Advantys OTB
Was this helpful?
What can we do to improve the information ?