Technical FAQs

Ask a Question

Do the Quantum PLCs support a Modbus Function Code 22 (16 Hex) Mask Write 4X Register request?

Yes, the Quantum PLCs do support a Modbus Function Code 22 (16 Hex) Mask Write 4X Register request?


Legacy KB System (APS) Data: RESL200689 V1.0, Originally authored by DiSa on 12/09/2009, Last Edited by DiSa on 12/09/2009
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?