Technical FAQs

Ask a Question

What is the part number of the DIO connector used in the TSXETG30xx ?

The TSXETG30xx comes with the DIO connector. But if the customer needs to replace the DIO connector, the part number is TSXETGACC01


Legacy KB System (APS) Data: RESL200525 V1.0, Originally authored by MiMe on 11/19/2009, Last Edited by MiMe on 11/19/2009
Related ranges: FactoryCast Gateway
Was this helpful?
What can we do to improve the information ?