Technical FAQs

Ask a Question

What is the maximum number of devices a TSXETG30xx can poll ?

The TSXETG30xx FactoryCast Gateway can poll up to 37 devices (up to 1000 variables).
Of these 37 devices, 31 of the devices can be on the Modbus serial link and only 5 devices can be on the ModbusTCP network.

Legacy KB System (APS) Data: RESL200524 V2.0, Originally authored by MiMe on 11/19/2009, Last Edited by BrWa on 11/17/2012
Related ranges: FactoryCast Gateway
Was this helpful?
What can we do to improve the information ?