Technical FAQs

Ask a Question

What is the maximum number of Modbus devices connected via the Modbus RS485 port for a TSXETG30xx ?

The TSXETG30xx FactoryCast Gateway can support up to 31 Modbus slave devices on the Modbus RS485 port.


Legacy KB System (APS) Data: RESL200478 V1.0, Originally authored by MiMe on 11/11/2009, Last Edited by MiMe on 11/11/2009
Related ranges: FactoryCast Gateway
Was this helpful?
What can we do to improve the information ?