Technical FAQs

Ask a Question

How do I wire unused channels on a 140ACI03000 card so I do not get the "F" indicator LED?

To eliminate the "F" indicator you will need to wire the unused channels voltage mode to the last channel in use. (See below ).


Legacy KB System (APS) Data: RESL2004 V2.0, Originally authored by RiVe on 10/09/2012, Last Edited by BrWa on 10/09/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?