Technical FAQs

Ask a Question

What is the difference between Vijeo Citect Unity Speedlink Dynamic and Unity Speedlink Static?

Vijeo Citect Unity Speedlink Dynamic is a tool used for linking to a Unity Pro .stu file project file. It makes a dynamic link between Vijeo Citect and the Unity project so that variables updates occur at Vijeo Citect side automatically from linked Unity project file.
Unity Speedlink Static tool is used for linking with a Unity .XSY file. It makes a static link between Vijeo Citect and Unity project so variable related updates has to be refreshed manually.

.


Legacy KB System (APS) Data: RESL200243 V1.0, Originally authored by MiMe on 10/14/2009, Last Edited by MiMe on 10/14/2009
Related ranges: Vijeo Citect
Was this helpful?
What can we do to improve the information ?