Technical FAQs

Ask a Question

What parameters can be saved by the keypad on a Altivar 71 ?

The keypad can save and transfer only the standard drive parameters and the parameters for the COM port (like CANopen, COM Scanner or Modbus).


Legacy KB System (APS) Data: RESL200241 V1.0, Originally authored by MiMe on 10/14/2009, Last Edited by MiMe on 10/14/2009
Related ranges: CANopen, Modbus
Was this helpful?
What can we do to improve the information ?