Technical FAQs

Ask a Question

How do you enable the Ethernet/IP profile on the Connexium TCSESM managed switches?

Goals and Symptoms

To explain the steps used to enable the Ethernet/IP profile on the Connexium TCSESM managed switches.

Facts and Changes

The Connexium TCSESM managed switches must be at a minimum firmware version 4.1 for this feature.

Procedure

First, log into the Connexium TCSESM managed switch as an administrator via the web pages.
Next, expand the Advanced heading on the browser tree and select Ethernet/IP. (see screenshot below)



Next, check the box next to Ethernet/IP to Enable the profile. (Step 2)
Finally, click the Set button to add to the switch configuration. (Step 3)

Remember to also save this configuration change so that this feature will be enabled after a power cycle.
To save this configuration change, select Load/Save on the top of the browser tree under Basic Settings.
Then click Save. (see screenshot below)


 


Legacy KB System (APS) Data: RESL200224 V1.0, Originally authored by MiMe on 10/13/2009, Last Edited by MiMe on 10/13/2009
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?